Swagelok® Source Inlet (SSI)
Swagelok® Source Inlet (SSI)
The source inlet establishes a connection between the high-pressure gas source and the distribution system. It is important the inlet is built with appropriate cylinder connections, hoses, tubing, filters, and vent, purge, and relief functions to ensure that gas can be safely fed into the primary gas pressure control or automatic changeover. For a single gas cylinder, the assembly can be as simple as a hose and connector, while multiple cylinders may require a manifold incorporating many hoses and valves.
We offer:
- Highly configurable options to purge or vent gases when changing bottles, always ensuring operator safety
- Available option to vent individual lines to maximize uptime
How Swagelok Advisors Can Help
It is easy to assume the source inlet will come standard with a new gas panel and will use the correct cylinder connector, but this is not always the case. Our advisors will ensure all componentry is included and correctly specified with minimal connection points, hoses that do not drop to the ground, and properly supported components. Additionally, we can advise when certain gases may require the use of special hoses.
Contact
For further details, please contact our Marketing Department at marketingbangalore@swagelok.com or call +91 80 42669253