Swagelok® Gas Panel (SGP)
Swagelok® Gas Panel (SGP)
As the primary gas pressure control, the SGP completes the first pressure reduction of the source gas and ensures it is delivered at the correct flow rate to the next stage of the system. Pressure reduction is accomplished in either one stage with a single pressure regulator or two stages through a dual pressure regulator arrangement.
We offer:
- Modular panels that are easy to service as any part can be detached via a Swagelok connection, so the panel never needs to be removed
- Options implemented around the regulator and valves for color-coding if required for your site
How Swagelok Advisors Can Help
Pinpointing correct inlet and delivery pressures can be difficult - our advisors will clearly explain considerations for different media. We can also help you understand where a two-stage regulator is required - many customers are surprised to learn most bottles do not require a twin-stage solution.
Contact
For further details, please contact our Marketing Department at marketingbangalore@swagelok.com or call +91 80 42669253